Technical FAQs

Ask a Question

Is an EZM1400TB Tap Box supplied with knockouts?

Yes, refer the attached CAD Drawing #: 3266 for locations and sizes of knockouts provided.
NOTE: When this device is installed outdoors, cable and conduit entry above live parts requires the use of UL Listed Liquid-Tight, or Water-Tight hubs.
This device is supplied with a Solid Top Endwall, Contractor to cut holes in Top Endwall for cable and conduit as required.

No. The top surface of the unit is blank, so for overhead feed, the user must use a proper hub and sealing arrangement, being careful to stay away from live parts.

CTA-ID : 2034574
Was this helpful?
What can we do to improve the information ?