Technical FAQs

Ask a Question

What are the catalog numbers for the stainless steel rod and stops in a 9049A6S Float Kit?

1091 S15 G1 Stainless Steel Stop
65006 006 01 Stainless Steel Set Screw
2-9049T1S 2 1/2 foot section of stainless steel rod and connector





CTA-ID : 2034138
Was this helpful?
What can we do to improve the information ?