Technical FAQs

Ask a Question

My LK3 disconnect switch is not getting continuity between L1 and T1. What could be the issue?

Look at the switch where the handle shaft goes in and there is a window that shows ``O`` for open or ``T`` for test. There is also an ``I``or on position which indicates when the main contacts are closed. It takes a lot of torque to get the contacts to the ``I`` or on position. When the contacts get to this position you will get continuity between L1 and T1.


CTA-ID : 2034516
Was this helpful?
What can we do to improve the information ?