Technical FAQs

Ask a Question

On a CU12L400FB, what is the difference between the Series M01 and M03 designs?

The difference is the meter socket used. The Series M01 design used a meter socket that was purchased from Cooper B-Line (part number 21324CD). The Series M03 design is using a meter socket that is manufactured by Square D Company (part number 73294-902-50). The meter sockets are not compatible between the two different designs.

CTA-ID : 2034478
Was this helpful?
What can we do to improve the information ?