Technical FAQs

Ask a Question

What is the standard lug kit used with NSJ600N and what wire size do the lugs accept?

Product Line:
Circuit Breakers

Environment:
Electrical Distribution Equipment

Resolution:
The standard lug kit 32510 includes 3 lugs that accept 2 cables per phase that are #2/0 AWG to 350 kcmil CU or 2 cables per phase that are #2/0 AWG to 500 kcmil AL


CTA-ID : 2034326
Was this helpful?
What can we do to improve the information ?