Technical FAQs

Ask a Question

Are E-Flex drives Service entrance rated?

E-Flex now provides a UL869A approved insulated ground neutral lug assembly mounting bracket with bonded enclosure ground wire that is suitable for use as service entrance equipment. This rating is available on Type 3R environmental ratings, specifically for frames B, C and D and was added with the Q2C/Product Selector.

CTA-ID : 2034835
Was this helpful?
What can we do to improve the information ?