Technical FAQs

Ask a Question

Do the last ``00`` digits on 9007 MS type limit switches, such as 9007MS03S0300 mean it has a bottom cable entrance?

Yes. The ``00`` at the end of the part number indicates a bottom entrance type of switch. Switches having a ``06`` suffix have a side cable entrance.


CTA-ID : 2034603
Was this helpful?
What can we do to improve the information ?