Technical FAQs

Ask a Question

Can a QO125, or any single-pole circuit breaker be used in Catalog # QO2TR?

The QO2TR is a 240 volt enclosure, and it is only for 2-pole circuit breakers only, because it has no neutral, and no neutral can be added in the Field.


CTA-ID : 2034817
Was this helpful?
What can we do to improve the information ?