Technical FAQs

Ask a Question

Can the obsolete EZMH113200 (Series M02) branch unit connect the current production EZM as listed in Digest 174?

Yes, the EZMH113220 branch unit is supplied with the same 1-Phase horizontal cross bus as used today (per Digest 174) and can connect to current 1-Phase mains and branch unts. Tenant circuit breakers Types suitable for use in this branch EZMH113200 branch unit have changed from the previous Types: Q2M, Q2M-VH or Q2MH (per Digest 172) to now be Types: QBP-TM, QDP-TM, QGP-TM (per Digest 174).


CTA-ID : 2034808
Was this helpful?
What can we do to improve the information ?