Technical FAQs

Ask a Question

Can a QO220HID breaker be used for High Magnetic applications? The application calls for a higher inrush characteristic in a two pole QO type breaker.

QO HID type breakers are optimized for High Intensity Discharge Lighting applications. The QO120HID and QO115HID are built with a higher magnetic withstand than the standard QO120 and QO115 breakers. The other HID breakers have the same trip curve as the standard.

CTA-ID : 2034831
Was this helpful?
What can we do to improve the information ?