Technical FAQs

Ask a Question

Where is the `Date Code` located on a QOC Load Center Cover?

It is near the UL Directory Label, and is very small numbers printed in black ink. If the numbers start with ``07`` this would mean it was manufactured in 2007. The complete date code would consist of six (6) numbers, such as: 072731.


CTA-ID : 2034793
Was this helpful?
What can we do to improve the information ?