Technical FAQs

Ask a Question

What is the Terminal Lug Data for a CH365AWK, Series E2 Heavy Duty safety switch?

The lugs on this device will accept (1) #1 AWG - 600 kcmil or (2) #1 AWG - 250 kcmil copper conductors per phase.

CTA-ID : 2035474
Was this helpful?
What can we do to improve the information ?