Technical FAQs

Ask a Question

What are the repair parts for a SU3040D300CB, Series M03?

NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED BELOW.
Only the parts listed below are considered field replaceable.
Meter Cover - 4056250650 Also requires insulator and rivets noted below.
Meter Cover Insulator - 4056138202 and Rivets (2) 2430313190
Meter Cover Mounting Screw - 4020513001K
Load Center Cover - 4056258950
Load Center Cover Mounting Screws - (3) 2142217101
Utility Pullbox Cover - 4056232801 (Handles not included, see below)
Utility Pullbox Cover Handles - (2) 2940101103 and Rivets (8) 2430315290
Utility Pullbox Cover Mounting Screws - (2) 4020513001K and (3) Sealing Screws X1299
Load Center Interior - 4056259050
Load Center Interior Mounting Screws - (6) 2142217101
Load Center Interior Lugs - (2) 4025116051 and Keps Nut (2) 2342702000
Interior Deadfront Trim - 4056232901
Interior Deadfront Trim Mounting Screws - 4020513001K
Meter Base Assembly - 7329490250
Mounting Channel - 4056142003
Factory Installed Main Breaker - QDL22200
Utility Lug Mounting Hardware - 4056211850
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED ABOVE.


CTA-ID : 2034424
Was this helpful?
What can we do to improve the information ?