Technical FAQs

Ask a Question

What is the part number for alternate lugs for an 800 amp MG I-line Main breaker that will accept (2) 600 kcmil cables /phase ?

Issue:
What is the part number for alternate lugs for an 800 amp MG I-line Main breaker that will accept  (2) 600 kcmil cables /phase ?

Product Line:
I Line panelboards.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
AL800P6K is a kit of 3 lugs. Each lug will accept (2) 3/0 AWG - 600 kcmil cables.


CTA-ID : 2034838
Was this helpful?
What can we do to improve the information ?