Technical FAQs

Ask a Question

9998PC242: Is the spring included with the contact kit?

Spring are not included in contact kit. Spring is part of the switch mechanism - 65079-502-51.


CTA-ID : 2034784
Was this helpful?
What can we do to improve the information ?