Technical FAQs

Ask a Question

What is the AIC rating of the main breaker in an EZM1400CB200?

65,000 RMS Symmetrical Ampere Short Circuit Current Rating at 240 VAC Maximum.
EZ Meter-Pak metering equipment is UL Listed as a Modular-Panelboard and has a meter center equipment rating as listed in Digest 174, Page 2-9 (see attachment).  EZ Meter-Pak is typically used to fed downstream Load Centers, refer to the attached Data Bulletin 4100DB0301R9/04 for appropriate Two Tier and Three Tier Short Circuit Current  Ratings.

CTA-ID : 2034777
Was this helpful?
What can we do to improve the information ?