Technical FAQs

Ask a Question

What is a "floating deadfront" on the flush covers used on QO and Homeline load centers?

Issue:
Product Design Features

Product Line:
Homeline Load centers

Environment:
Cover features

Cause:
Application

Resolution:
The "floating deadfront' piece is considered an 'Automatic flush adjustment', which takes up the spacing between the branch breaker faces and the deadfront piece with any adjustments required by the installer, when the enclosure is mounted flush in the wall. This is standard on ALL Homeline load center combination covers(use for both flush and surface mount applications) and the QO Flush covers.


CTA-ID : 2034442
Was this helpful?
What can we do to improve the information ?