Technical FAQs

Ask a Question

Is replacement control coil available for 8903PBQ10V38?

The V38 voltage code is for a 120/208 volt coil. For the 8903PB contactors this dual voltage coil is obsolete and replaced by either a 120 volt coil or a 208 volt coil. The 120 volt replacement coil is 9998PBV02 and the 208 volt replacement coil is 9998PBV08. The replacement coils include both solenoid and rectifier.


CTA-ID : 2034642
Was this helpful?
What can we do to improve the information ?