Technical FAQs

Ask a Question

For an existing 9001B control station with a pilot light, is it possible to replace just the 120V pilot light lamp with a 277V lamp?

No. Only a 120 volt pilot light is available in the 9001B stations.

CTA-ID : 2034941
Was this helpful?
What can we do to improve the information ?