Technical FAQs

Ask a Question

What are the repair parts for the CH221NRB, series F5? (may be shown as F05)

The repair parts for the CH221NRB, series F5 (F05) are as follows. No other parts are available.

Line Base Assembly -40566-422-50 (requires one per switch. Arc suppressor assembly not included)
Load Base Assembly - 40566-410-50 (requires one per switch)
Arc Suppressor Assembly - 40560-018-01 (requires one per switch)
Lug Assembly - 40251-016-52 (per lug)
Switch Mechanism - 40566-107-50
Handle Assembly - 4056684150K
Handle Gasket - 40566-031-01
Lockplate - 40566-376-01
Neutral Assembly - CSN03 (includes mtg. hardware and bonding screw)
Neutral Bonding Screw - Contact (888) SQUARED for further assistance.
Line & load base mounting screw - 40205-160-01 (3 required for line & 2 required for load base)
Arc suppressor mounting screw - 40205-145-01 (1-required)
Lockplate mounting screw - 22999-405-62 (2 required)

CTA-ID : 2034619
Was this helpful?
What can we do to improve the information ?