Search FAQs
Are EDB, EGB, and EJB breakers HID rated?
Product Line:
Circuit Breakers
Resolution:
1, 2, and 3 pole EDB, EGB, and EJB breakers from 15 A to 50 A are UL listed as HID (high intensity discharge) rated.
Breakers listed for HID will have the marking "HID" on the breaker itself. As an example, see the below picture.
Circuit Breakers
Resolution:
1, 2, and 3 pole EDB, EGB, and EJB breakers from 15 A to 50 A are UL listed as HID (high intensity discharge) rated.
Breakers listed for HID will have the marking "HID" on the breaker itself. As an example, see the below picture.
Released for:Schneider Electric USA
Explore more
Range:
Explore more
Range: