Technical FAQs

Ask a Question

XU8B18NP340D. What is the ``D`` stand for?

``D`` means the sensor has a 4 pin M12 DC micro connector. It has M12x1.0 threads and is an IEC standard for DC sensors. In the upcoming line of global detection products, the ``D`` code will be replaced by ``M12`` [e.g: XUB9B1PAM12].


CTA-ID : 2034582
Was this helpful?
What can we do to improve the information ?