Technical FAQs

Ask a Question

Can you get an overcurrent trip switch (SDE) in the Powerpact M frame breaker?

Yes. This became available around February 2007. It was not available prior to this date. To verify acceptability, customers can verify by the presence or absence of the black SDE plug. The plug blocked the installation of the SDE. On the newer breakers, the changes include removal of this black plug. The SDE is located between the handle and the shunt trip pocket.

CTA-ID : 2034580
Was this helpful?
What can we do to improve the information ?