Technical FAQs

Ask a Question

Does the XPSAC5121 have a PE ground pin? The wiring diagram shows the PE to ground termination, but the the device does not have this feature nor marking on it.

The 24 volt units do not have Potential Earth grounding termination. The wiring diagram is generic and shows the 120 and 240 volt units.


CTA-ID : 2034566
Was this helpful?
What can we do to improve the information ?