Technical FAQs

Ask a Question

Are the QO and Homeline surgebreakers rated for UL C62 lightning arresting

This device is dual rated as a surge arrestor and TVSS transient suppression. It meets UL C62-41 and C62-45 ratings, as well as, UL E1449 listing


CTA-ID : 2034671
Was this helpful?
What can we do to improve the information ?