Technical FAQs

Ask a Question

What is the maximum size of wire that can be used with a H100XFA?

Use a #3 AWG, 75 degree C, copper wire for 100 ampere rating.


CTA-ID : 2034504
Was this helpful?
What can we do to improve the information ?