Technical FAQs

Ask a Question

Are the NSJ type breakers fire pump rated?

This type of breaker is UL489 rated, and so therefore are suitable for use in fire pump applications.


CTA-ID : 2034507
Was this helpful?
What can we do to improve the information ?