Technical FAQs

Ask a Question

What is the catalog number for mounting feet for 3 pole QOU breaker

Issue:
What is the part number for mounting feet for 3 pole QOU breaker

Product Line:
QOU Circuit Breaker

Environment:
Product sold in North America

Cause:
Need to mount a QOU breaker without a DIN rail.

Resolution:
Use the QOUMF3 kit. Contains 1 piece. (Two mounting feet required per circuit breaker)
For bulk packs: QOUMF3B - 24 pieces

For more information on QOU accessories, see QOU Catalog:  0720CT9401, page 14.
CTA-ID : 2033780
Was this helpful?
What can we do to improve the information ?