Technical FAQs

Ask a Question

What is the Terminal Lug Data for a H365 and H365N, Series E2 or E4 Heavy Duty safety switch?

Product Feature

Product Line:
Safety Switch

Clarifying lug wire range

The lugs on this device will accept (1) #1/0 AWG - 750 kcmil or (2) #1/0 AWG - 300 kcmil aluminum or copper conductors per phase.

CTA-ID : 2033732
Was this helpful?
What can we do to improve the information ?