Technical FAQs

Ask a Question

What does the suffix 1366 mean?

A circuit breaker with a 1366 suffix consists of 2A/2B (1352) auxiliary switch in the right pole and 1A (2100) alarm switch. This is UL approved.


CTA-ID : 2033632
Was this helpful?
What can we do to improve the information ?