Technical FAQs

Ask a Question

Can you use a HOA with the U-Line starter using a multifunction Programmable Unit LUCM and the communication modules LULC### along with the pre-wired coil connector?

You will not be able to use the prewired bus assembly with a HOA. If a manual operated HOA is required it must be hardwired into the wiring scheme interrupting the coil terminal A1 and A2 .



CTA-ID : 2033618
Was this helpful?
What can we do to improve the information ?