Technical FAQs

Ask a Question

Can the HQO adpaters for I-Line use QO GFI or EPD type breakers?

Product Line:
I-Line, QO Breakers

Resolution:
The HQO units will accept up to 4 GFI breakers and 2 standard breakers. It has a total of 6 breaker slots of which the middle 4 may be used for GFI/EPD breakers.
 
Was this helpful?
What can we do to improve the information ?