Technical FAQs

Ask a Question

Can the QO318L200G, Fixed Main Lugs load center, be converted to a Main Circuit Breaker load center?

Issue:
product features

Product Line;
QO load centers

Environment;
Convert to main breaker

Cause:
Application

Resolution;
This is a fixed Main Lug load center and is not convertible to Main Breaker load center.

 
Was this helpful?
What can we do to improve the information ?