Technical FAQs

Ask a Question

<br /><br />Customer ordered a 80084150-013 float to use with a 9035 float switch. The float is tapped at the top what are the threads size?

The threaded piece that screws into the float comes with the 9049DCA2 and is no longer available


CTA-ID : 2033672
Was this helpful?
What can we do to improve the information ?