Technical FAQs

Ask a Question

What is the wire range for the compression lug supplied in an H8LKE2 lug kit?

Issue:
Wire range accommodated by lug

Product Line:
HD Safety Switches

Environment:
Installation

Cause:
Wire range

Resolution: 
Each compression lug will accept (1) 500 - 750 kcmil aluminum or (1) 500 kcmil copper conductor.
Three lugs are supplied per connector assembly and two connector assemblies are supplied per H8LKE2 kit.
One kit will supply three compression lugs for the line and load side of one switching pole or neutral of the 800A switch.
The compression lug supplied is an Anderson VCEL07512H1.
H8LKE2
Safety Switch information here.
 
Was this helpful?
What can we do to improve the information ?