Technical FAQs

Ask a Question

Why does the FAL32100 require a minimum air gap of 0.68 inches between the enclosure cover and the top face of the breaker?

This is to prevent a ground-strike during an interruption. If the gap is going to be less than 0.68 inches, the customer needs to supply a fiber insulator between the breaker and enclosure cover.

CTA-ID : 2033459
Was this helpful?
What can we do to improve the information ?