Technical FAQs

Ask a Question

8536SF: Is a 24V AC coil available for the Size 4 starter?

24V coil not available. 120V is the lowest voltage coil available for the Size 4 starter. The customer could use an interposing relay if necessary.


CTA-ID : 2033391
Was this helpful?
What can we do to improve the information ?