Technical FAQs

Ask a Question

What is the standard lug wire size for QMB225W, QMB325W, QMB365W fusible switches?<br /><br />

Standard AL/CU lugs accepts (2) -3/0 - 600 kcmil per phase. However due to NEC wire bending criteria the lug is to accept (2) 3/0 - 500 kcmil per phase. Lug catalog number is 40251-287-50.

CTA-ID : 2033381
Was this helpful?
What can we do to improve the information ?