Technical FAQs

Ask a Question

What comes with the NQOD225SFL kit?

What comes with the NQOD225SFL kit:

Product Line:
NQOD panelboards that were sold and supported in the USA.

Product clarification.

Catalog component identification.

The kit comes with (2) 3 inch rail extensions, (1) 3 inch deadfront extension, (4) lugs.

Lug wire range is (2) #4 - 300kcmil per phase and neutral

NOTE:  The NQOD225SFL kit is now obsolete, with no replacement. 

CTA-ID : 2033455
Was this helpful?
What can we do to improve the information ?