Technical FAQs

Ask a Question

What is the difference between a KAL36070 and a FAL36070?

Difference between a FA and KA frame breaker.

Product Line:
Legacy Breakers

Electrical Distribution Equipment

Interchanging of the FA and KA breakers

A FAL Breaker is a 100A Frame and a KAL Breaker is a 250A Frame.  Breaker will have different foot print since the frame size is different.

CTA-ID : 2033335
Was this helpful?
What can we do to improve the information ?