Technical FAQs

Ask a Question

What are the repair parts for the QMB222TW switch Series E1?

Only the parts listed below are field replaceable in a QMB222TW twin switch:
Load base assembly - 40560-026-50 (Includes lugs and clips). There is one base per switch unit (two units per switch assembly).
Arc Shield /Suppressor Assembly - 40512-534-50. One per switch unit.
Handle Knob Kit - 40283-437-50.
Lug Assembly (Per Lug) - 40251-016-52
Lug Mounting Screw - 40205-154-01




CTA-ID : 2033275
Was this helpful?
What can we do to improve the information ?