Technical FAQs

Ask a Question

Is the Q1100AN a forked type or a straddle type lug?

Issue:
Product Features

Product Line:
Load Center Accessory

Cause:
Product features

Resolution:
The Q1100AN is a forked type lug. 


CTA-ID : 2033543
Was this helpful?
What can we do to improve the information ?