Technical FAQs

Ask a Question

Are the Mini Power Zone Transformers rated for 50 and 60 Hertz applications?

Transformers must be chosen to operate on either 60 Hz or 50 Hz or both

Product Line:
LV Transformers

Applies to Mini Power Zone Transformers by SquareD/Schneider Electric

Transformers are rated at either 60 Hz or 50 Hz or both


The Mini Power Zone Transformers found in the Digest are rated for 60 Hertz power sources only. Custom units may be quoted through the local SquareD/Schneider Electric Distributor/Field Office.

CTA-ID : 2033535

Was this helpful?
What can we do to improve the information ?