Technical FAQs

Ask a Question

Why are the XA2B and XB2B push buttons becoming obsolete on June 30, 2007 ? <br />

In September 1999 the Harmony push button line was launched and the conversion has been taking place ever since . As of 3/07 , 75% of 22mm customers are buying new Harmony XB4 and XB5 products . The Harmony line offers many advantages over the old line and will become RoHS compliant in the 2nd quarter of 2007 . The old product/s are not and cannot become RoHS compliant . Tooling on the old product/s is wearing out and the global volume is not great enough to invest in new tooling . Except for SE-NAOD , rest of the world has converted ( 97-99%) .

CTA-ID : 2033519
Was this helpful?
What can we do to improve the information ?