Technical FAQs

Ask a Question

Is it permitted to use a three pole fusible switch, such as a QMB361TW in a single phase application, even though it is a three phase device?

You can use a three pole QMB361TW in a single phase QMB panel. The bus spacing is the same for both single and three phase. One of the phase connectors would not be used.


CTA-ID : 2033614
Was this helpful?
What can we do to improve the information ?