Technical FAQs

Ask a Question

What are the dimensions of the FAL and the GJL breakers?

The FAL is 6 in H 4.5 in W 4.13 in D.
The GJL is 4.72 in H 3.54 in W 3.94 in D

CTA-ID : 2033468
Was this helpful?
What can we do to improve the information ?