Technical FAQs

Ask a Question

What are the repair parts for a QO412L200, Series G1, Three-phase Load Center?

Only the parts listed below are considered field replaceable.
Cover - QOC412LF/S
Interior Assembly - QON412L200
Neutral Bonding hardware - 4028330450
Main Lugs - 4025116251
Neutral Assembly - SN12200
Indoor Cover mounting screw - 4020513002K
The following parts are obsolete and no longer available:
Indoor cover door hinge - 173132
Indoor cover latch ring - 186012
Indoor cover latch spring - 163471




CTA-ID : 2033464
Was this helpful?
What can we do to improve the information ?