Technical FAQs

Ask a Question

DZ2FR1: What is the torque for the lug mounting bolts and nuts in this lug kit?

The 12 mm hardware supplied with the kit: 515 lb.-in. or 58 N-m
Second jam nut used to secure the anti-rotation plate: 60 lb.-in. or 6.77 N-m
See Instruction Sheet 30072-451-70 for more details

CTA-ID : 2033556
Was this helpful?
What can we do to improve the information ?