Technical FAQs

Ask a Question

What is the difference between a XB6AA25A and XB6AA25B shown in the Digest?<br /><br />

Suffix is for contact block arrangement, in this case PC board mounting is designated with ``A`` and quick connect, solder type ``B.`` . Customer can only get break out parts to build XB6AA25A and they are:
ZB6AA2 operator
ZB6E1A normally open contact block
ZB6AE1 normally closed contact block
ZB6Y011 PC mounting collar

CTA-ID : 2033509
Was this helpful?
What can we do to improve the information ?