Technical FAQs

Ask a Question

What are the repair parts for a SMS368W, Series E1 (E01)?

Only the parts listed below are considered field replaceable:
Complete Arc Suppression Assembly - 2 part numbers required:
Arc Suppressor Assembly (3 per switch) - 4052031850
Arc Shield (3 per switch) - 4052085601
Load Base Assembly (3 per switch, includes lugs) - 4052052550
Load Base Mounting Screw (3 required per load base) - 2142720241
Handle Knob Kit - 4028343550
Lug Assembly (per lug) - 4025128750
Lug Mounting Nut (per lug) - 2342702400




CTA-ID : 2033274
Was this helpful?
What can we do to improve the information ?